Part Number: AM625
你好
环境:CCS: 12.6.0
SDK: mcu_plus_sdk_am62x_08_06_00_18
在 例程 M4 核 gpio 外部中断工程中,board.c 文件在创建中断过程时报错:sciclient event config failed ,可能是哪方面配置错误?
感谢感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于sciclient event config failed报错,您可以尝试参考下面链接:
e2e.ti.com/.../mcu-plus-sdk-am243x-am243x-lp---gpio-interrupt-sciclient-event-config-failed-error
你好:
我重新安装了MCU的SDK编译工程gpio_input_interrupt_am62x-sk_m4fss0-0_nortos_ti-arm-clang后,使用ccs的debug后出现如下错误。
CortexA53_0: File Loader: Verification failed: Values at address 0x0000000000000001 do not match Please verify target memory and memory map.
CortexA53_0: GEL: File: D:\CCS\gpio_input_interrupt_am62x-sk_m4fss0-0_nortos_ti-arm-clang\Debug\gpio_input_interrupt_am62x-sk_m4fss0-0_nortos_ti-arm-clang.out: a data verification error occurred, file load failed.