am335x用sd卡启动后,应如何从sd卡烧写程序到emmc。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,Jian Zhou,
这是用sd卡升级的打印,请帮忙分析下,谢谢。
U-Boot 2015.07-00114-gf5078ef-dirty (Jan 25 2016 - 10:43:00 +0800)
Watchdog enabled
I2C: ready
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
71471840 bytes read in 3963 ms (17.2 MiB/s)
32990 bytes read in 47 ms (684.6 KiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x44292e0 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff4000, end 8ffff0dd ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.1.6-g52c4aa7 (kevin@kevin) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #1 PREEMPT Mon Jan 25 10:55:52 CST 2016
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x BeagleBone Black
[ 0.000000] cma: Reserved 24 MiB at 0x9e800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=00000000-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 417776K/524288K available (6247K kernel code, 254K rwdata, 2096K rodata, 67820K init, 229K bss, 81936K reserved, 24576K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc082e05c (8345 kB)
[ 0.000000] .init : 0xc082f000 - 0xc4a6a000 (67820 kB)
[ 0.000000] .data : 0xc4a6a000 - 0xc4aa9b28 ( 255 kB)
[ 0.000000] .bss : 0xc4aac000 - 0xc4ae57f8 ( 230 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000031] clocksource timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000041] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000206] Console: colour dummy device 80x30
[ 0.000228] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000233] This ensures that you still see kernel messages. Please
[ 0.000238] update your kernel commandline.
[ 0.000255] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089326] pid_max: default: 32768 minimum: 301
[ 0.089419] Security Framework initialized
[ 0.089466] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089474] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090088] Initializing cgroup subsys blkio
[ 0.090110] Initializing cgroup subsys memory
[ 0.090147] Initializing cgroup subsys devices
[ 0.090160] Initializing cgroup subsys freezer
[ 0.090172] Initializing cgroup subsys perf_event
[ 0.090193] CPU: Testing write buffer coherency: ok
[ 0.090557] Setting up static identity map for 0x80008200 - 0x80008270
[ 0.091932] devtmpfs: initialized
[ 0.100003] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.107382] omap_hwmod: tptc0 using broken dt data from edma
[ 0.107480] omap_hwmod: tptc1 using broken dt data from edma
[ 0.107563] omap_hwmod: tptc2 using broken dt data from edma
[ 0.111831] omap_hwmod: debugss: _wait_target_disable failed
[ 0.166167] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.168134] pinctrl core: initialized pinctrl subsystem
[ 0.169268] NET: Registered protocol family 16
[ 0.171225] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.199316] cpuidle: using governor ladder
[ 0.229306] cpuidle: using governor menu
[ 0.232306] OMAP GPIO hardware version 0.1
[ 0.240099] No ATAGs?
[ 0.240129] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.276239] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.278887] vgaarb: loaded
[ 0.279431] SCSI subsystem initialized
[ 0.279904] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.280044] pps_core: LinuxPPS API ver. 1 registered
[ 0.280051] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.280079] PTP clock support registered
[ 0.280783] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.280976] Advanced Linux Sound Architecture Driver Initialized.
[ 0.281689] Switched to clocksource timer1
[ 0.290463] NET: Registered protocol family 2
[ 0.291197] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.291242] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.291280] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.291359] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.291375] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.291519] NET: Registered protocol family 1
[ 0.291933] RPC: Registered named UNIX socket transport module.
[ 0.291946] RPC: Registered udp transport module.
[ 0.291952] RPC: Registered tcp transport module.
[ 0.291958] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 4.291021] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
[ 4.291081] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 4.293035] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 4.293117] audit: initializing netlink subsys (disabled)
[ 4.293185] audit: type=2000 audit(4.290:1): initialized
[ 4.299423] VFS: Disk quotas dquot_6.6.0
[ 4.299609] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 4.301461] NFS: Registering the id_resolver key type
[ 4.301528] Key type id_resolver registered
[ 4.301537] Key type id_legacy registered
[ 4.301599] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 4.304092] NET: Registered protocol family 38
[ 4.304158] io scheduler noop registered
[ 4.304171] io scheduler deadline registered
[ 4.304225] io scheduler cfq registered (default)
[ 4.305140] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 4.306818] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 4.307740] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 4.310753] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 155, base_baud = 3000000) is a 8250
[ 4.946532] console [ttyS0] enabled
[ 4.950909] [drm] Initialized drm 1.1.0 20060810
[ 4.955917] slave hdmi: could not get i2c
[ 4.968929] brd: module loaded
[ 4.976386] loop: module loaded
[ 4.980353] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 4.988680] mousedev: PS/2 mouse device common for all mice
[ 4.994386] i2c /dev entries driver
[ 4.998757] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 5.079054] mmc0: host does not support reading read-only switch, assuming write-enable
[ 5.087419] ledtrig-cpu: registered to indicate activity on CPUs
[ 5.093880] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 5.099756] mmc0: new high speed SDHC card at address 0001
[ 5.106228] mmcblk0: mmc0:0001 SD 3.69 GiB
[ 5.111555] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 5.119272] remoteproc0: wkup_m3 is available
[ 5.123950] mmcblk0: p1 p2
[ 5.127602] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 5.136772] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 5.148486] remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2
[ 5.161922] oprofile: using arm/armv7
[ 5.165920] Initializing XFRM netlink socket
[ 5.170244] NET: Registered protocol family 17
[ 5.174814] remoteproc0: Falling back to user helper
[ 5.180115] NET: Registered protocol family 15
[ 5.184819] Key type dns_resolver registered
[ 5.189355] omap_voltage_late_init: Voltage driver support not added
[ 5.197291] ThumbEE CPU extension supported.
[ 5.203659] Registering SWP/SWPB emulation handler
[ 5.238681] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 5.244130] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 5.373926] tda998x 0-0070: found TDA19988
[ 5.378998] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 5.385696] [drm] No driver support for vblank timestamp query.
[ 5.392027] tilcdc 4830e000.lcdc: No connectors reported connected with modes
[ 5.399207] [drm] Cannot find any crtc or sizes - going 1024x768
[ 5.413704] Console: switching to colour frame buffer device 128x48
[ 5.425294] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 5.430909] tilcdc 4830e000.lcdc: registered panic notifier
[ 5.461725] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 5.531709] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 5.537843] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 5.548841] libphy: 4a101000.mdio: probed
[ 5.553049] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 5.563074] cpsw 4a100000.ethernet: Detected MACID = 78:a5:04:dc:33:42
[ 5.570562] hctosys: unable to open rtc device (rtc0)
[ 5.579032] ALSA device list:
[ 5.582202] No soundcards found.
[ 5.585770] Warning: unable to open an initial console.
[ 5.675171] Freeing unused kernel memory: 67820K (c082f000 - c4a6a000)
[ 5.681898] mmc1: MAN_BKOPS_EN bit is not set
[ 5.691827] mmc1: new high speed MMC card at address 0001
[ 5.697817] mmcblk1: mmc1:0001 MMC04G 3.65 GiB
[ 5.702684] mmcblk1boot0: mmc1:0001 MMC04G partition 1 1.00 MiB
[ 5.708759] mmcblk1boot1: mmc1:0001 MMC04G partition 2 1.00 MiB
[ 5.716973] mmcblk1: p1 p2
[ 7.312541] remoteproc0: failed to load am335x-pm-firmware.elf
[ 7.318535] remoteproc0: powering up wkup_m3
[ 7.345149] remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2
[ 7.741854] remoteproc0: Falling back to user helper
[ 8.937149] remoteproc0: request_firmware failed: -11
[ 9.006744] remoteproc0: rproc_boot failed
[ 9.208202] EXT4-fs (mmcblk1): VFS: Can't find ext4 filesystem
[ 9.215152] EXT3-fs (mmcblk1): error: can't find ext3 filesystem on dev mmcblk1.
[ 9.223618] EXT2-fs (mmcblk1): error: can't find an ext2 filesystem on dev mmcblk1.
[ 9.233381] FAT-fs (mmcblk1): bogus number of reserved sectors
[ 9.239472] FAT-fs (mmcblk1): Can't find a valid FAT filesystem
[ 9.268248] cramfs: wrong magic
[ 9.272968] FAT-fs (mmcblk1): bogus number of reserved sectors
[ 9.279007] FAT-fs (mmcblk1): Can't find a valid FAT filesystem
[ 9.366531] EXT4-fs (mmcblk0): VFS: Can't find ext4 filesystem
[ 9.413708] EXT3-fs (mmcblk0): error: can't find ext3 filesystem on dev mmcblk0.
[ 9.429594] EXT2-fs (mmcblk0): error: can't find an ext2 filesystem on dev mmcblk0.
[ 9.461088] FAT-fs (mmcblk0): bogus number of reserved sectors
[ 9.492292] FAT-fs (mmcblk0): Can't find a valid FAT filesystem
[ 9.584606] cramfs: wrong magic
[ 9.589944] FAT-fs (mmcblk0): bogus number of reserved sectors
[ 9.642092] FAT-fs (mmcblk0): Can't find a valid FAT filesystem
[ 10.270538] EXT4-fs (mmcblk1p1): VFS: Can't find ext4 filesystem
[ 10.282764] EXT3-fs (mmcblk1p1): error: can't find ext3 filesystem on dev mmcblk1p1.
[ 10.293382] EXT2-fs (mmcblk1p1): error: can't find an ext2 filesystem on dev mmcblk1p1.
[ 10.309944] FAT-fs (mmcblk1p1): bogus number of reserved sectors
[ 10.337087] FAT-fs (mmcblk1p1): Can't find a valid FAT filesystem
[ 10.362018] EXT4-fs (mmcblk1p2): recovery complete
[ 10.366867] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 10.394093] EXT4-fs (mmcblk1boot0): VFS: Can't find ext4 filesystem
[ 10.400804] EXT4-fs (mmcblk1boot1): VFS: Can't find ext4 filesystem
[ 10.430208] EXT3-fs (mmcblk1boot0): error: can't find ext3 filesystem on dev mmcblk1boot0.
[ 10.439230] EXT3-fs (mmcblk1boot1): error: can't find ext3 filesystem on dev mmcblk1boot1.
[ 10.475195] cramfs: wrong magic
[ 10.482034] FAT-fs (mmcblk1p1): bogus number of reserved sectors
[ 10.490745] EXT2-fs (mmcblk1boot0): error: can't find an ext2 filesystem on dev mmcblk1boot0.
[ 10.500193] EXT2-fs (mmcblk1boot1): error: can't find an ext2 filesystem on dev mmcblk1boot1.
[ 10.515742] FAT-fs (mmcblk1p1): Can't find a valid FAT filesystem
[ 10.533851] FAT-fs (mmcblk1boot0): bogus number of reserved sectors
[ 10.540732] FAT-fs (mmcblk1boot1): bogus number of reserved sectors
[ 10.553031] FAT-fs (mmcblk1boot0): Can't find a valid FAT filesystem
[ 10.559677] FAT-fs (mmcblk1boot1): Can't find a valid FAT filesystem
[ 10.652993] cramfs: wrong magic
[ 10.658422] cramfs: wrong magic
[ 10.662283] FAT-fs (mmcblk1boot0): bogus number of reserved sectors
[ 10.668991] FAT-fs (mmcblk1boot0): Can't find a valid FAT filesystem
[ 10.676151] FAT-fs (mmcblk1boot1): bogus number of reserved sectors
[ 10.689093] FAT-fs (mmcblk1boot1): Can't find a valid FAT filesystem
[ 10.745068] kjournald starting. Commit interval 5 seconds
[ 10.753789] EXT3-fs (mmcblk0p2): using internal journal
[ 10.779466] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 13.001737] random: nonblocking pool is initialized
我在论坛上也看到过有人提到这个问题,我是用sdk自带的工具代码包是ti-processor-sdk-linux-am335x-evm-02.00.00.00-Linux-x86-Install.bin
看log应该是没有做文件系统,你需要把emmc进行格式化到相应的文件系统格式(fat, ext3/ext4).
可以参考 http://processors.wiki.ti.com/index.php/Sitara_Uniflash_Flash_Programming_with_Linux?keyMatch=uniflash%20AM335x&tisearch=Search-EN#eMMC_Programming_Process 中的脚本文件
我的那篇文档是基于SDK06的,建议你先下载SDK06试一下。