This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不是的,我利用的是sysbios6 用CCS6进行开发,里面不是可以直接进行配置,另外我也试过了利用starterware里面的C源码,进行了CP15MMUEnable();CacheEnable(CACHE_ALL);这两个操作 我主频设置的是550Mhz 有个问题想请教一下,CCS 利用sysbios里面不是直接可以利用脚本进行配置的吗?
并且这边用的是starterware里面的GEL文件,这个DDR3配置没有出错,程序可以正常烧写调试,但是运行的速度比较慢,测试大概只有5M使能CAChe后的,对了,您那边能否提供一下MMU 和CACHE的配置,我这边使能MMU 和CACHE的配置是参考了help文件里面的介绍的,是能够MMU应该没有出错,因为如果不映射地址,是访问不了寄存器,使能了CACHE之后,速度也略有提升,但是提升不高