Other Parts Discussed in Thread: AM1808
你好!我现在用am1808的emif口作为数据总线传输信号,数据位宽为16bit。将ASIZE设置为16-bit data bus,发现在读写的时候,每读写一次读写使能信号出现使能两次。比如我在读的时候,用示波器抓取CS使能信号及WE使能信号,读一次,在CS使能期间,会出现两次WE使能。另外我将ASIZE设置为8-bit data bus,读一次,在CS使能期间,会出现四次WE使能。然后我将ASIZE设置为2时,读一次,在CS使能期间,就只会出现一次WE使能,但是低位地址线EMA_BA就被禁止了。请问是不是还有其他地方需要配置数据宽度,使得数据位宽为16bit时,只出现一次读写使能?
下面是ASIZE配置
ASIZE 0-3h Asynchronous Data Bus Width. This field defines the width of the asynchronous device's data bus.
0 8-bit data bus
1h 16-bit data bus
2h-3h Reserved
另外,SDRAM Configuration Register (SDCR)中有个NM参数,改变这个设置也没有任何变化
NM Narrow mode bit. This bit defines whether a 16- or 32-bit-wide SDRAM is connected to the EMIFA.
This bit field must always be set to 1. Writing to this field triggers the SDRAM initialization
sequence.
0 32-bit SDRAM data bus is used.
1 16-bit SDRAM data bus is used.