This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于 USB DEV MSC



startware 中的块大小为512字节,按TIwiki上说:

The default block size is 512 bytes. If the alternate block media has a different block size, then this must be updated in the USB stack. This can be achieved by updating macros DEVICE_BLOCK_SIZE and MAX_TRANSFER_SIZE with the new block size.

修改块为2048字节,修改

1. ramdisk.c

#define RAM_DISK_SIZE (1024 * 1024 * 16)
#define LBA_SIZE 2048
#define TRANSFER_SIZE 2048

2.usbdmsc.h

#define DEVICE_BLOCK_SIZE   2048

3.cppi41dma.h

#define USB_PACKET_LENGTH                2048

#define MAX_TRANSFER_SIZE       USB_PACKET_LENGTH

#define USB_PACKET_LENGTH                512

#define MAX_TRANSFER_SIZE       2048

都是不行的;

如果不修改第3步,则能识别,但格式化提示错误。