Part Number: TDA4VPE-Q1
Regarding the EPWM function of TDA4VPE, I have the following points to confirm:
- Pin Configuration: Does TDA4VPE only support PWM output through the six groups of EPWM0~5 IOs? Are there any other pins supporting this function?
- Output Differences: What is the functional difference between EHRPWM Output A and Output B for EPWM0~5?
- Complementary/Independent Operation: Are Output A and Output B two complementary PWM signals controlled by the same timer? Can they also be configured as two independent PWM outputs?
- Multi-Channel Synchronization: For these six groups (12 PWM outputs), can combinations (e.g., pairwise or triple-group) share a common timer to synchronize timing and adjust phase for driving brushed motors, three-phase BLDC motors, or four-phase five-wire stepper motors? Example: Combining EPWM0 Output A and EPWM1 Output A.