This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM6678L开发板的USB Emulator Error



用一块TDMSEVM6678L的开发板。

按照光盘里的文档,把CCS5.2以及一些驱动,都缺省正确安装了。

板子上电后,USB连接电脑后显示XDS100 + RS232 V1.0 。。。

打开CCS,一个工程,连接配置选的是TI XDS2XXUSB Onboard Emulator /IcePick D,

debug在连接emulator时报错。

错误是:

Error initializing emulator

(Error -2083@0x0)

Unable to ....

(Emulation package 5.0.838.0)

我重启了CCS、电脑,都不能解决问题。

请问该如何解决这个问题?

谢谢!

  • 应该是你选择的连接类型不正确,我手上没有6678的EVM板,但是从wiki上的信息看应该选择

    Select the connection type as "Texas Instruments XDS100v1 USB Emulator" for XDS100 or "Blackhawk XDS560v2-USB Mezzanine Emulator" for XDS560 in the drop down list

    6678的EVM有两种,TMDSEVM6678L使用的是XDS100v1 USB Emulator,另一种TMDXEVM6678LXE/LE 使用的是Blackhawk XDS560v2-USB Mezzanine Emulator",你首先需要明确你使用的EVM的类型

    具体步骤参考http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_Getting_Started_Guide

  • 谢谢!

    换了 连接类型,可以了。