IDK4379EVM(R1.3版本)的Endat2.2接口部分,芯片SN65HVD78的供电为3.3V。而在IDDK379的Endat2.2电路部分采用的是5V供电,通过TXB0104进行了5V和3.3V的电平转换。而在海德汉的Endat2.2的手册中,编码器的供电为5V,但是并没有指明其信号部分的电平要求。
我的问题是:
Endat的信号接口到底应该采用3.3V电平还是5V电平?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.