This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCIEVMK2LX 开发板怎么都连不上!!!



刚买了两块 TCIEVMK2LX  开发板,1周过去了,程序都还没有下进去。

现象是这样的:

    1)  安装开发套件中提供的CCV5.5,发现不支持开发板6630芯片。
在官网下载了CCS6.1.2,mcsdk_3_01_04_07,支持6630芯片,据说使用开发板上自带胡xds2xx,可以不用linsence,也就没有添加。
        加电后,安装XDS2XX的驱动,使用了开发套件中U盘提供的  CP210x_VCP_Drivers,按照getting_started 下载最新的驱动,但都无法连接、识别下载器。
   分别在win7和winxp系统下进行了尝试,winxp系统下没有任何反馈信息,win7系统下打印一堆(截图见附件)
//////////////////////////////////////////////

[Start: Texas Instruments XDS2xx USB Debug Probe_0]

 Execute the command:

 %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

 [Result]

 -----[Print the board config pathname(s)]------------------------------------

 C:\Users\jm433\AppData\Local\TEXASI~1\CCS\

  ti\0\0\BrdDat\testBoard.dat

 -----[Print the reset-command software log-file]-----------------------------

 This utility has selected a 560/2xx-class product.

This utility will load the program 'xds2xxu.out'.

E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io

Failed to open i/o connection (xds2xxu:0)

 An error occurred while soft opening the controller.

 -----[An error has occurred and this utility has aborted]--------------------

 This error is generated by TI's USCIF driver or utilities.

 The value is '-250' (0xffffff06).

The title is 'SC_ERR_ECOM_EMUNAME'.

 The explanation is:

An attempt to access the debug probe via USCIF ECOM has failed.

 [End: Texas Instruments XDS2xx USB Debug Probe_0]

/////////////////////////////////

 我的问题是:

    1) 开发套件中的软件CCS5.5,是否不支持开发板芯片6630,是否需要下载新版本的软件?
    2) 如上面的现象,究竟是什么问题,如何才能在TCIEVMK2LX开发板上下载程序,并调试?
请各位大侠帮忙!!!!!!!!!!
截图.zip