This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VC5509A调试时,连接不上仿真器



大家新年好!!

  第一次玩VC5509A,使用XDS100V1仿真器,编译器为CCS V6。

最初连接仿真器时,没有连接两个EMU脚,运行第二条语句时就跑飞了,后来以为是没有连接全部引脚的问题,就把所有的都连接上了。

提示如下:

C55xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located. (Emulation package 5.1.641.0) 



谢谢大家