DM8168使用DVRRDK4.0开发做三路输出:HDMI,DVO2,SD
板子输入信号是1080I60
输出:HDMI -> 1080P60,DVO2 -> 1080I60,SD-> PAL
HDMI和SD这两路输出正常,但是DVO2这一路无显示,输出信号错误
DVO2这一路使用VOUT0输出,设置内同步
我将输入信号设置为绿屏测试,VOUT0输出信号应该是除了行头有1之外全部为0,但是实际测试中,VOUT0的16根线有的是这样,有的却不是,输出数据错误
请问,这是怎么回事?DM8168的DVO2使用需要配置什么?需要注意什么?是不是链里需要修改什么?