This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问,为什么TI-RTOS for C6000不能显示driver?



软件安装都是在c:\ti目录下。

CCS6.0.0.00190

XDCTOOLS 3_30_04_5_2

TI-RTOS for C6000 2_00_01_23

安装之后,打开example工程,用的C66XX MultiCore的6678,工程的cfg文件打开后却没有看到driver项。driver就是手册上的EMAC, I2C, SPI, 等等等。

我重新用命令build 了TI_RTOS for CCS,如上操作,仍然看不到各个driver项目。

安装了rtos for MPS430,然后打开example工程后,却可以看到driver项。

请问是软件工具有什么问题?

还是rtos for c6000本身就是没有driver?

谢谢!