This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748的GPIO无法控制NAND Flash的写保护引脚



您好!

    在6748的系统中,我使用下拉电阻将NAND FLash的WP#引脚连接到地,再将WP#连接到6748的GPIO0_0上,再设置GPIO0_0为普通输出方式,输出高电平,用万用表测后发现WP#上电平为1.1V左右,即无法拉高,然后我将WP#上的下拉电阻去掉,设置GPIO0_0为推挽输出,发现无论设置输出为高还是低,WP#引脚上的电平始终为3.3V;如果设置GPIO0_0带上拉电阻输出,则无论设置该引脚输出高低,WP#始终为高;如果设置GPIO0_0带下拉电阻输出,则无论设置该引脚输出高低,WP#始终为低,使用的NAND芯片型号为MX30LF2G28AB-TI,查看数据手册,并无对WP#引脚有特殊说明;在断电下检测WP#引脚对地的电阻,为400K左右,电路中拿掉的下拉电阻为10K。

    请问这可能是哪里的问题?