各位专家好!
EDMA在进行link传输的时候,交替加载两组参数通过一个通道进行传输,我现在设置了两个源地址和两个目的缓冲区,交替往两个目的缓冲区传送数据,我希望的是在pong后回到ping 但是实际是触发第一次完成ping触发第二次完成了pong但触发第三次第四次都是pong,请问是什么原因呢?如果要达到希望的效果,应该做些什么修改?谢谢!
/**
* @file edma_test.c
*
* @brief
*
*/
#include <stdio.h>
#include <ti/csl/csl_edma3.h>
#include <ti/csl/csl_edma3Aux.h>
#include <ti/csl/csl_cache.h>
#include <ti/csl/csl_cacheAux.h>
/**********************************************************************
************************** Global Variables **************************
**********************************************************************/
/* Global Variables which are used to dump the TPCC register overlay in the
* debugger... */
CSL_TpccRegs* gEDMACC0Regs = (CSL_TpccRegs*)CSL_EDMA0CC_REGS;
CSL_TpccRegs* gEDMACC1Regs = (CSL_TpccRegs*)CSL_EDMA1CC_REGS;
CSL_TpccRegs* gEDMACC2Regs = (CSL_TpccRegs*)CSL_EDMA2CC_REGS;
/* Global Buffers (Source and Destination) for PING-PONG */
Uint8 srcBuff1[512];
Uint8 srcBuff2[512];
Uint8 dstBuff1[512];
Uint8 dstBuff2[512];
/**********************************************************************
************************ EDMA TEST FUNCTIONS *************************
**********************************************************************/
/**
* @b Description
* @n
* This is the example routine which perform EDMA ping pong buffer transfer
* where channel is open in the global region.
* It implements following steps
* - Intializes and Opens the EDMA Module .
* - Sets up the interrupt for the EDMA global region.
* - Sets up the EDMA module using the API csl_edma3Hwsetup ()
* - Enables the EDMA global region
* - Opens the channel 'channelNum' get the param handle for PARAM 1, 2
* - PING is mapped to PARAM Entry 1
* - PONG is mapped to PARAM Entry 2
* - PING is Linked with PONG...
* - Enables the EDMA interrupt using CSL_EDMA3_CMD_INTR_ENABLE.
* - Enables Interrupt (Bit 0-2) for the global region interrupts
* - Manually triggers the DMA channel 'channelNum'(This should be PING)
* - Polls on IPR bit 0 (Since TCC for PING is 0)
* - Clear the pending bit
* - Manually triggers the channel 'channelNum' (This should be PONG)
* - Polls on IPR bit 1 (Since TCC for PONG is 1)
* - Clears the pending bit
* - Compares the data in the destination buffer is proper or not.
* - Closes the EDMA module and channel.
*
* @param[in] instNum
* EDMA Instance Number on which the test is executed.
* @param[in] channelNum
* EDMA Channel Number on which the test is executed
*
* @retval
* Success - 0
* @retval
* Failure - <0
*/
static Int32 edma_ping_pong_xfer_gbl_region (Int32 instNum, Uint8 channelNum)
{
CSL_Edma3Handle hModule;
CSL_Edma3Obj edmaObj;
CSL_Edma3ParamHandle hParamPing;
CSL_Edma3ParamHandle hParamPong;
CSL_Edma3ChannelObj chObj;
CSL_Edma3CmdIntr regionIntr;
CSL_Edma3ChannelHandle hChannel;
CSL_Edma3ParamSetup myParamSetup;
CSL_Edma3Context context;
CSL_Edma3ChannelAttr chAttr;
CSL_Status status;
Uint32 loopIndex;
/* Start the EDMA PING-PONG test over the Global Region. */
printf ("Debug: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d...\n", instNum, channelNum);
/* Initialize data */
for (loopIndex = 0; loopIndex < 256; loopIndex++)
{
srcBuff1[loopIndex] = loopIndex;
srcBuff2[loopIndex] = loopIndex;
dstBuff1[loopIndex] = 0;
dstBuff2[loopIndex] = 0;
}
/* Module initialization */
if (CSL_edma3Init(&context) != CSL_SOK)
{
printf ("Error: EDMA module initialization failed\n");
return -1;
}
/* Open the EDMA Module using the provided instance number */
hModule = CSL_edma3Open(&edmaObj, instNum, NULL, &status);
if ( (hModule == NULL) || (status != CSL_SOK))
{
printf ("Error: EDMA module open failed\n");
return -1;
}
/* Channel open */
chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL;
chAttr.chaNum = channelNum;
hChannel = CSL_edma3ChannelOpen(&chObj, instNum, &chAttr, &status);
if ((hChannel == NULL) || (status != CSL_SOK))
{
printf ("Error: Unable to open EDMA Channel:%d\n", channelNum);
return -1;
}
/* Change Channel Default queue setup from 0 to 3 */
if(0)//if (CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_3) != CSL_SOK)
{
printf ("Error: EDMA channel setup queue failed\n");
return -1;
}
/* Map the DMA Channel to PARAM Block 2. */
CSL_edma3MapDMAChannelToParamBlock (hModule, channelNum, 2);
/* Obtain a handle to parameter set 2 */
hParamPing = CSL_edma3GetParamHandle(hChannel, 2, &status);
if (hParamPing == NULL)
{
printf ("Error: EDMA Get Parameter Entry failed for 2.\n");
return -1;
}
/* Obtain a handle to parameter set 1 */
hParamPong = CSL_edma3GetParamHandle(hChannel, 1, &status);
if (hParamPong == NULL)
{
printf ("Error: EDMA Get Parameter Entry failed for 1.\n");
return -1;
}
/* Setup the parameter entry parameters (Ping buffer)//CSL_EDMA3_STATIC_EN我修改 */
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN, \
0, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_DIS, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff1;
myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(256,1);
myParamSetup.dstAddr = (Uint32)dstBuff1;
myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,1);
myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);
myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);
myParamSetup.cCnt = 1;
/* Ping setup */
if (CSL_edma3ParamSetup(hParamPing,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
}
/* Pong setup */
myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN,\
1, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_EN, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff2;
myParamSetup.dstAddr = (Uint32)dstBuff2;
myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPing,0);
if (CSL_edma3ParamSetup(hParamPong,&myParamSetup) != CSL_SOK)
{
printf ("Error: EDMA Parameter Entry Setup failed\n");
return -1;
}
//ZW added to keep the coherience between L1D and L2(MSM). Jun 1 2012
CACHE_wbInvAllL1d(CACHE_NOWAIT);
CACHE_wbInvAllL1dWait();
/* Interrupt enable (Bits 0-1) for the global region interrupts */
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0x3;
regionIntr.intrh = 0x0000;
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,®ionIntr);
/* Trigger channel 111111111111111*/
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0;
regionIntr.intrh = 0;
/* Poll on IPR bit 0 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x1));
/* Clear the pending bit清除挂起位 */
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,®ionIntr);
/* Trigger Channel222222222222222 */
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
/* Poll on IPR bit 2 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x2));
for (loopIndex = 0; loopIndex < 256; loopIndex++)
{
dstBuff1[loopIndex] = 0;
dstBuff2[loopIndex] = 0;
}
/* Clear the pending bit清除挂起位 */
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,®ionIntr);
/* Trigger Channel 33333333333333*/
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
regionIntr.region = CSL_EDMA3_REGION_GLOBAL;
regionIntr.intr = 0;
regionIntr.intrh = 0;
/* Poll on IPR bit 0 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x1));
/* Trigger Channel 44444444444444*/
CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
/* Poll on IPR bit 2 */
do {
CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,®ionIntr);
} while (!(regionIntr.intr & 0x2));
/* Close channel */
if (CSL_edma3ChannelClose(hChannel) != CSL_SOK)
{
printf("Error: EDMA Channel Close failed\n");
return -1;
}
/* Close EDMA module */
if (CSL_edma3Close(hModule) != CSL_SOK)
{
printf("Error: EDMA Module Close failed\n");
return -1;
}
/* The test passed. */
return 0;
}
/**
* @b Description
* @n
* Entry point for the test code.
*
* @retval
* Not Applicable.
*/
void main (void)
{
Uint8 channelNum;
// Int32 regionNum;
Uint8 instNum = 0;
printf ("**************************************************\n");
printf ("******************* EDMA Testing *****************\n");
printf ("**************************************************\n");
/* EDMA Instance 0: Supports only 16 DMA Channels. */
for (channelNum = 0; channelNum < 16; channelNum++)
{
if (edma_ping_pong_xfer_gbl_region(instNum, channelNum) < 0)
{
printf ("Error: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d FAILED\n", instNum, channelNum);
return;
}
printf ("Debug: Testing EDMA(%d) Ping-Pong Test (Global) Region for Channel %d Passed\n", instNum, channelNum);
}
printf ("**************************************************\n");
printf ("************* EDMA Testing Successful ************\n");
printf ("**************************************************\n");
return;
}