我现在有个项目是需要用到每个DSP片子的唯一序列ID号(具体用途不便说明),不知C6678有没有相应的寄存器???
6678 evm开发板电路图上使用的NAND FLASH 和 Nor Flash 这两款flash芯片出厂有唯一的序列号或者产品序列ID,每块片子都是唯一的,我现在想尽可能的通过DSP片子的寄存器进行唯一区分,不想使用片外的flash进行识别区分,麻烦各位大神提供解决方案
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,6678手册
Each device has a unique MAC address. There are two registers to hold these values, MACID1 (0x02620110) and MACID2 (0x02620114).
前面有用户说发现有不唯一的MACID,请确定是否把两个寄存器的值都读出来了。
如果真的发现有不唯一的MACID而且又是正常渠道购买可以联系TI或代理商。