This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 PCIE 读取PC端数据失败



各位好:

现在我们在调试C6678与PC通过PCIE通信,目前遇到的问题如下:

DSP启动方式为PCIe BOOT,配置为EP模式。

PC可以往DSP内存读写数据,而DSP无法通过EDMA或者Memcpy读取PC的内存数据,获取的数据全部是0。

我们做了如下几种尝试:

1、PC驱动直接配置DSP EMDA读取PC内存数据,连接仿真器看EDMA是配置成功的,EDMA也启动了,但是观察到目的地址的数据全部是0.

2、直接运行DSP程序启动EDMA,情况与1相同。

3、DSP使用Memcpy读取DSP内存,同样观察到DSP的目的地址的数据全部是0.

以上尝试我们都查看了OB_OFFSET_INDEXn(0x21800200200+N*8)等寄存器的值都是正确配置的。

请问有人遇到过相同的问题了吗?这是由于什么问题导致的?有什么方法可以解决,该问题已经困惑快2周时间了,谢谢大家了