This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6748无法连接仿真器



现有一块6748的板子,同一块板子,不同时间做的,以前做的都能正常连上560仿真器,现在做的怎么都连不上,量测1.2V,1.8V,3.3V的电源都正常,RESET信号也正常,24M晶振也起振,连接仿真器出错,信息如下:

Error connecting to the target:
Error 0x80000240/-1146
Fatal Error during: Initialization, OCS,
Invalid data was scanned by the emulation controller.
Verify the board setup to make sure the scan chain is properly
defined.
If the setup is correct, then RESET EMULATOR.  This will disconnect each
target from the emulator.  The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.



Board Name: OMAPL138_TIXDS560
Cpu Name: C6400PLUS_0

Abort:        Close Code Composer Studio.
Retry:        Try to connect to the target again.
Cancel:        Remain disconnected from the target
Diagnostic:    Run diagnostic utility.

请问是什么问题