数据源是电脑VGA信号,通过TVP7002采集,1920*1080分辨率,现在PCLK=148.5MHZ,水平同步信号67.5KHZ,垂直刷新60HZ
由于水平同步和垂直同步信号是直接连接DM368,而TVP7002出来的并行信号先通过了SN74CBT16214DGGR多路数据选择器(同时也是缓存器)进入到
DM368,所以现在出现了帧数据不同吧的情况,主要影响的是67.5KHZ的水平同步信号,最终导致实际图像水平抖动而且实际图像被左右挤在一起了。
我想知道DM368的VPFE是不是有类似于提前或者延后的时间变量用于这种情况下的帧同步。即推迟或者延后多少个时钟周期去重新重新同步水平和垂直信号。