This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6638 CCS5.4连接不上仿真器



最近在用 spectrum digital XDS560 V2 STM Emulator做tracePod, CCS版本是5.4,DSP型号:TCI6638. 在用CCS做test connection时,总是会出现如下错误:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]

-----[Print the board config pathname(s)]------------------------------------

C:\DOCUME~1\TDLTE-~1\LOCALS~1\APPLIC~1\.TI\

    693494126\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.

This utility will load the program 'sd560v2u.out'.

Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\xds560v2pro.xsvf

The library build date was 'Apr  2 2013'.

The library build time was '00:13:51'.

The library package version is '5.1.73.0'.

The library component version is '35.34.40.0'.

The controller does not use a programmable FPGA.

E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Receive::dtc_io

E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Receive::dtc_io

E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Send::dtc_io

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-252' (0xffffff04).

The title is 'SC_ERR_ECOM_OPERATE'.

The explanation is:

An attempt to operate the USCIF interface via USCIF ECOM has failed.

[End]

不知道这个错误代码-252表示什么意思