This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下:SD卡启动系统,卡在了 emoteproc0: failed to load am335x-pm-firmware.elf

Other Parts Discussed in Thread: TPS65910

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.1.13-g8dc6617 (root@ppa2001-HP-Z220-SFF-Workstation) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #4 PREEMPT Fri Mar 4 09:56:51 CST 2016
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM
[ 0.000000] cma: Reserved 24 MiB at 0x9e800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=00000000-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 485372K/524288K available (6207K kernel code, 241K rwdata, 2096K rodata, 260K init, 227K bss, 14340K reserved, 24576K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc082402c (8305 kB)
[ 0.000000] .init : 0xc0825000 - 0xc0866000 ( 260 kB)
[ 0.000000] .data : 0xc0866000 - 0xc08a2728 ( 242 kB)
[ 0.000000] .bss : 0xc08a5000 - 0xc08ddd88 ( 228 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000030] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000078] clocksource timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000104] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000475] Console: colour dummy device 80x30
[ 0.000530] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000546] This ensures that you still see kernel messages. Please
[ 0.000561] update your kernel commandline.
[ 0.000600] Calibrating delay loop... 298.59 BogoMIPS (lpj=1492992)
[ 0.067680] pid_max: default: 32768 minimum: 301
[ 0.067940] Security Framework initialized
[ 0.068054] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.068081] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.069661] Initializing cgroup subsys blkio
[ 0.069719] Initializing cgroup subsys memory
[ 0.069817] Initializing cgroup subsys devices
[ 0.069858] Initializing cgroup subsys freezer
[ 0.069891] Initializing cgroup subsys perf_event
[ 0.069953] CPU: Testing write buffer coherency: ok
[ 0.070703] Setting up static identity map for 0x80008200 - 0x80008270
[ 0.074214] devtmpfs: initialized
[ 0.103859] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.129919] omap_hwmod: tptc0 using broken dt data from edma
[ 0.130228] omap_hwmod: tptc1 using broken dt data from edma
[ 0.130499] omap_hwmod: tptc2 using broken dt data from edma
[ 0.137994] omap_hwmod: debugss: _wait_target_disable failed
[ 0.207861] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.212587] pinctrl core: initialized pinctrl subsystem
[ 0.215454] NET: Registered protocol family 16
[ 0.221202] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.247762] cpuidle: using governor ladder
[ 0.277744] cpuidle: using governor menu
[ 0.286797] OMAP GPIO hardware version 0.1
[ 0.308226] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_default, deferring probe
[ 0.315871] No ATAGs?
[ 0.315930] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.379428] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.389723] vgaarb: loaded
[ 0.390894] SCSI subsystem initialized
[ 0.392130] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.392254] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.392614] media: Linux media interface: v0.10
[ 0.392791] Linux video capture interface: v2.00
[ 0.392921] pps_core: LinuxPPS API ver. 1 registered
[ 0.392940] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.393021] PTP clock support registered
[ 0.395014] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.397298] Switched to clocksource timer1
[ 0.424848] NET: Registered protocol family 2
[ 0.426802] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.426942] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.427063] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.427238] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.427440] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.427851] NET: Registered protocol family 1
[ 0.428641] RPC: Registered named UNIX socket transport module.
[ 0.428672] RPC: Registered udp transport module.
[ 0.428690] RPC: Registered tcp transport module.
[ 0.428706] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.430612] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
[ 0.430719] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.435657] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.435862] audit: initializing netlink subsys (disabled)
[ 0.436015] audit: type=2000 audit(0.420:1): initialized
[ 0.456462] VFS: Disk quotas dquot_6.6.0
[ 0.457007] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.462980] NFS: Registering the id_resolver key type
[ 0.463146] Key type id_resolver registered
[ 0.463170] Key type id_legacy registered
[ 0.463338] jffs2: version 2.2. (NAND) (SUMMARY) 漏 2001-2006 Red Hat, Inc.
[ 0.469734] NET: Registered protocol family 38
[ 0.469898] io scheduler noop registered
[ 0.469935] io scheduler deadline registered
[ 0.470067] io scheduler cfq registered (default)
[ 0.472645] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.478985] backlight supply power not found, using dummy regulator
[ 0.481970] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 0.484473] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.493832] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 155, base_baud = 3000000) is a 8250
[ 1.169262] console [ttyS0] enabled
[ 1.175006] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 156, base_baud = 3000000) is a 8250
[ 1.187105] [drm] Initialized drm 1.1.0 20060810
[ 1.193011] panel panel: pins are not configured
[ 1.200948] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.207830] [drm] No driver support for vblank timestamp query.
[ 1.273615] Console: switching to colour frame buffer device 100x30
[ 1.293775] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.299438] tilcdc 4830e000.lcdc: registered panic notifier
[ 1.327383] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.359915] brd: module loaded
[ 1.375791] loop: module loaded
[ 1.381393] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.457378] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.463548] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 1.471736] libphy: 4a101000.mdio: probed
[ 1.475799] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Atheros 8031 ethernet
[ 1.486841] cpsw 4a100000.ethernet: Detected MACID = 68:c9:0b:c8:03:22
[ 1.498203] mousedev: PS/2 mouse device common for all mice
[ 1.503902] i2c /dev entries driver
[ 1.510809] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.662115] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.672904] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.682578] remoteproc0: wkup_m3 is available
[ 1.687087] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 1.696469] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 1.707573] remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2
[ 1.716272] remoteproc0: Falling back to user helper
[ 1.723483] oprofile: using arm/armv7
[ 1.728287] Initializing XFRM netlink socket
[ 1.732683] NET: Registered protocol family 17
[ 1.737262] NET: Registered protocol family 15
[ 1.742622] Key type dns_resolver registered
[ 1.747753] omap_voltage_late_init: Voltage driver support not added
[ 1.754888] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
[ 1.763929] cpu cpu0: cpu0 clock notifier not ready, retry
[ 1.770427] ThumbEE CPU extension supported.
[ 1.774815] Registering SWP/SWPB emulation handler
[ 1.785188] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.790721] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.799945] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xda
[ 1.806386] nand: Micron MT29F2G08ABAEAWP
[ 1.810634] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 1.818492] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.824052] 10 ofpart partitions found on MTD device 8000000.nand
[ 1.830252] Creating 10 MTD partitions on "8000000.nand":
[ 1.835710] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.843683] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.852019] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.860338] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.868661] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[ 1.877180] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 1.885552] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 1.893893] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 1.902732] 0x000000200000-0x000000a00000 : "NAND.kernel"
[ 1.913698] 0x000000a00000-0x000010000000 : "NAND.file-system"
[ 2.037711] tps65910 0-002d: No interrupt support, no core IRQ
[ 2.045047] tps65910 0-002d: Error in configuring external control EN1
[ 2.051742] tps65910 0-002d: Failed to initialise ext control config
[ 2.058842] vrtc: failed to enable
[ 2.062557] tps65910 0-002d: failed to register tps65910-pmic regulator
[ 2.069347] tps65910-pmic: probe of tps65910-pmic failed with error -121
[ 2.076875] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.086264] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 2.094650] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 2.128151] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
[ 2.136968] cpu cpu0: cpu0 clock notifier not ready, retry
[ 2.143467] hctosys: unable to open rtc device (rtc0)
[ 2.156967] wlan-en-regulator: disabling
[ 2.161135] lis3_reg: disabling
[ 2.164334] vbat: disabling
[ 2.168719] Waiting for root device PARTUUID=00000000-02...
[ 61.737675] remoteproc0: failed to load am335x-pm-firmware.elf
[ 61.743711] remoteproc0: powering up wkup_m3
[ 61.748405] remoteproc0: Direct firmware load for am335x-pm-firmware.elf failed with error -2
[ 61.757075] remoteproc0: Falling back to user helper
[ 107.657345] random: nonblocking pool is initialized
[ 121.757538] remoteproc0: request_firmware failed: -11
[ 121.762727] remoteproc0: rproc_boot failed