This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
DVR RDK4.01有一个额外的NVR的包,里面有基于live555的RTSP实现。但UI部分,还是UDworks的版权,TI没有相关源码。
Lu Kingkuang,
不知道你说的把IPNC sdk在DVR rDK上跑起来是什么意思?IPNC RDK和DVR RDK的软件并不兼容。建议你一个为基础,然后把另外一个不同的link/驱动挪过来,测试运行。TI并没有测试过这样情况。
DVR RDK2.0版本太旧了,建议使用最新版本,新版本修正了一个bug,也添加了不少新的功能。
我的意思是将../DVRRDK_04.00.00.03/dvr_rdk/dvrapp(包含NVR的app和gui代码)和../DVRRDK_04.00.00.03/dvr_rdk/dvrapp/module(包含live555代码)两个目录内容copy到../DVRRDK_02.00.00.23/dvr_rdk/路径下,重新编译/DVRRDK_02.00.00.23,是否就可以跑NVR的demo用例了,还是要做什么修改?
另外,请问DVRRDK_04.00.00.03软件包是否可以在原来的DM8168开发板(配套提供的还是DVRRDK_02.00.00.23开发包)上正常运行起来?
现在要再买一套DM8168开发板+DVRRDK_04.00.00.03软件包,费用不少啊!
谢谢!
Lu Kingkuang,
TI任何版本的DVR RDK都是可以在TI官方的DM816x EVM加上相关子卡上运行起来的。
DVR RDK2.x和DVR RDK4.01版本差距太大,无法估计NVR代码在老版本软件上运行是否会有问题,你只能自己试试。
今天将../DVRRDK_04.00.00.03/dvr_rdk/dvrapp(包含NVR的app和gui代码)和../DVRRDK_04.00.00.03/dvr_rdk/dvrapp/module(包含live555代码)两个目录内容copy到../DVRRDK_02.00.00.23/dvr_rdk/路径下,参照《DM8168 DVR RDK Application and GUI Guide》手册编译application(make dvrapp),但是报下面的error:
请问这些未定义的结构体/宏 是不是在DVRRDK_04.00.00.03中新定义的,而/DVRRDK_02.00.00.23中没有?
...
app_decproc.c:35: error: 'VDEC_CHN_CREATE_PARAMS_S' undeclared (first use in this function)
app_decproc.c:95: error: 'VDEC_FRAMELEVELPROCESSCALL' undeclared (first use in this function)
app_decproc.c:99: error: 'VDEC_MAX_BUFFERS_IN_QUEUE' undeclared (first use in this function)
app_decproc.c:106: error: 'VDEC_DECODE_I_ONLY' undeclared (first use in this function)
...