显示的错误信息如下:
Error connecting to the target:
Error 0x80002240/-116 Fatal Error during: Initialization, OCS, Control,
This error was generated by TI's USCIF driver.
SC_ERR_CTL_TRASH <-116>
A bad parameter value was detected within an internal data-structure of Unified-SCIF.
The controller or Unified-SCIF may be in an invalid state.
Sequence ID: 0
Error Code: -116
Error Class: 0x80002240