This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[求助]如何使用SEED XDS560V2在TMDXEVM8148上connect dsp(Error -1146)



仿真器为:SEED XDS560V2

www.seeddsp.com/showgongju.php

开发板为:TMDXEVM8148,开发商mistralsolutions

www.mistralsolutions.com/.../tmdxevm8148.html

已经根据SEED emulator installation guide成功安装emulator驱动,并在CCS v5 New Target Configuration 中的Connect找到SEED XDS560V2 USB Emulator。

 

Here is my  procedure:

1.Install the emulator driver

2.Choose a  project, build it and  New a Target Configuration file, 

   in basic tag, "connection", choose "SEED XDS560V2 USB Emulator". in "Board or Device", choose "EVMDM8148"

   in Advanced tag, click C674X_0, in initialization script, choose"PG2.1_DM814X_20Mhz_Si.gel.gel", which is support from Mistral.

   click CortexA8, choose the same gel file,

   save.

3.Connect the Jtag emulator with PC and board, click "Debug",

4.Debug session launched, then ERROR,

and I can not connect the ARM core, just hint error connecting to the target then go back go the CCS edit perspective.

在CCS v5下Debug,然后提示出错,console错误如下:

Error connecting to the target:
(Error -1146 @ 0x0)
Device ID is not recognized or is not supported by driver. 
Confirm device and emulator configuration is correct, or update device driver.
(Emulation package 5.0.681.0)
请问Target Configuration中的选项是否正确?

感谢技术支持人员!