This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在Linux下用xds100v2调试335x,速度非常慢,从连接、执行gel、单步调试,每一个操作都非常卡,单步走一步需要15~20秒才反应过来,这是正常的么?
我的环境是:
Ubuntu 12.04 64bit
am3352
CCS 6
原版的XDS100v2
应该还不至于这么慢,在windows上试过吗?
还有你是用的虚拟机吗?
Despite some configurations work fine with XDS100 on a virtual machine, the performance degradation is significant and should be expected, especially with more intricate ISAs such as C66x and ARM cores.
我用的是虚拟机,VMWare 12
我另外有闻亭的TDS560USB,不知道是否支持linux下使用,ccs如何能够支持呢? 如果可以的话应该速度也会有改善吧
现在这个仿真器速度太慢,linux启动一点输出都没有,电路和原版改动非常大,想debug具体定位下问题都不行,卡在这里了
XDS100本身在windows下就很慢,在虚拟机下就会更慢,建议还是用560吧
1. 560 usb 需要有ccs的license, 请您先确定是否有license。 560 快点。
2. 不要用虚拟机,直接用windows下更好啊。