(Error -120 @ 0x0)
This error number is used when a command is invalid.
It is likely a problem with `SC_CMD' in SMG_call()
selecting a function that has not been implemented.
(Emulation package 5.1.641.0)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
(Error -120 @ 0x0)
This error number is used when a command is invalid.
It is likely a problem with `SC_CMD' in SMG_call()
selecting a function that has not been implemented.
(Emulation package 5.1.641.0)
Wang Xin,
请参考下面的内容:
http://wiki.tiprocessors.com/index.php/Debugging_JTAG_Connectivity_Problems#Invalid_parameters_or_command
谢谢你,我询问了仿真器的客服人员,ccs6.1确实不能兼容我的仿真器驱动,我已经换成5.5了