使用了一段时间的TMDSEVM6678LE评估板,有以下几个疑问:
1 在LE评估版上有两个仿真器:XDS100V1和XDS560V2,按照《TMDXEVM6678L_QSG_v_1.0》上配置好串口后与评估板上boot mode开关,上电后串口会输出相应内容,在调试PC的硬件管理器中可以看到“usb serial port(com4)”;采用同样的配置,仅将调试U口插在XDS560V2仿真器上,即使用XDS560V2在线调试,上电后串口不输出任何内容,在调试PC的硬件管理器中也看不到“usb serial port(com4)”;为什么使用XDS560V2仿真器不能发现串口“usb serial port(com4)”?
2 在使用开发板对文档《BiosMulticoreSDK_2.0_UserGuide》中“Example 1 - Building and running a simple single core application”实例进行学习时,在执行“Select Target->Connect Target to connect to the core”步骤时,仅在使用XDS560V2仿真器才可以连接上CORE,使用XDS100V1执行该操作会报错“Error connecting to the target: cannot access register at 0x00000000 (Error -2131) @0 (0x0)”
3 在哪里可以获取下列外设CSL配置与使用的DEMO:SRIO,SPI,EMIF16。
4 若使用XDS560PLUS仿真器对6678LE评估版进行在线调试,在XDS560PLUS仿真器14pin接口与评估板上60pin引脚间应该怎么处理?若在自己设计的使用6678板上,使用XDS560PLUS仿真器时14pin应该怎么与6678引脚对应?
谢谢各位专家