你好!今天使用6678EVM的时候突然评估板自带的仿真器无法与PC进行连接。初步认为电脑的驱动等都没有问题,问题最有可能是XDS560v2仿真器。
整个评估板通电后,XDS560v2仿真器上的LED灯:D2(黄色),D3(绿色),一段时间后只有D3(绿色,不断闪烁)。使用CCSv5的Test Connect进行测试,显示无法找到仿真器。信息如下:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\PC\AppData\Local\.TI\213602635\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
Download failed for file C:\ti\ccsv5\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
[End]
请问这样的问题该如何解决,查找了许多方法,都没有效果。是不是仿真器的硬件出了问题?
另外麻烦告知一下TI 6678的售后技术服务维修该怎么弄。