我用的是合众达510plus仿真器,ccs5.5 目标板是seed-dec6437 ,配置文件test connection时出错
错误代码是
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\ly\AppData\Local\.TI\2526794187\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'seedjca8990isa.dll'.
The library build date was 'Aug 20 2013'.
The library build time was '22:56:19'.
The library package version is '5.1.232.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '1' (0x00000001).
The controller has an insertion length of '16' (0x00000010).
This utility will attempt to reset the controller.
A error occurred while attempting to reset the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-342' (0xfffffeaa).
The title is 'SC_ERR_HUNG_COMMAND'.
The explanation is:
Failure due to the controller command-finish taking too long.
[End]
看了一些其他人也有这些问题,但是没有人给出解决办法,希望大家看看有办法解决吗?