因项目需求,需要在dm368上获取1080P-YUV420、1080P-YUV422以及D1-YUV420, 目前从前端sensor捕获的为RAW数据,使用RSZ会影响效率,不能满足要求,请问各位大神们,在不影响效率的情况有什么比较好的方案没?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
YN,
DM36x的DDR资源是很有限的。请问你的1080p是多少帧?获取的YUV420数据是都编码么?那YUV42数据的用途是什么?
注意IPNC软件支持1080p+D1@30f/s需要在486Mhz的DM36x上才刚刚够。你的应用不光要看效率问题,还要看系统的DDR资源是否够用。
你好,
dm368支持1080p么?
从VPBE的手册里,只能看到支持1080i,搜索不到1080p的信息。
:)谢谢
你好,
硬件上输出的lcd接口可支持1080p30。注意,显示会消耗很多DDR, 系统上能否正常,还要看你的应用场景。
编码支持1080p和显示支持是不同的概念。
孟工,你好!
1.那如果想要配置为1080p显示,如何与手册里1080i的描述去配置来适应呢?
另外,DVSDK包4.02里面没有找到1080p相关的驱动,是否有相应的驱动实例呢?
2.因为我们没有连接field信号,所以1080i是不是不行了呢?如果要尝试BT656的方式来显示,是否可以?有没有相应的驱动?
3.请帮忙再看下视频采集偏右哪个问题,目前尝试了一些方法,还未定位。
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/103814.aspx
谢谢:)
你好,
请问1080p的输出是数字输出么?你准备解码加显示么?
Feller,
DM36x的DDR带宽很有限,你的use case是存在风险的。
1080p的LCD时序是可以根据LCD接口后面器件/芯片的需要来配置的。BT656是8-bit带宽,如果要发送1080p30,VPBE的PCLK是无法支持的。注意,如果VPBE的PCLK大于27Mhz,需要外部输入时钟给VPBE。