自己做的板子,ARM核能正确连接并且运行程序,ARM的Boot方式选择的从NAND Flash中Boot,DSP核连接不上,显示信息如下,DSP核选的Boot方式是由ARM核Boot,具体的错误信息如下,这种情况该怎么解决??
Error connecting to the target:
(Error -1137 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package 5.1.232.0)