This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dsp 接口问题请教



打算使用C67XX系列, 有如下几个问题请教下,谢谢!

1.  MCASP和McBSP使用有什么区别?

2. MCASP速度可以达到多少?(我指的速率是每秒传多个16bit数据);如果EMIF时钟是10M,那以16bit为一个单位的话,速度还不到1M,我看了手册上UART的速度可以达到12Mbps,这么换算的话EMIF不是速度还低于UART?如果用EMIF接口,线比较多,用那种排线的可靠传输距离是多少?

3. 674x和C6713比性能上有多大差别?价格上对比如何?

4.6000系列的是不是都没有片内flash,是否需要扩展片外flash?现在我的单板外围设备就有了MCBSP接口,FLASH接口,DDR接口,UART接口或者EMIF接口或者MCASP接口,这些接口应该都要驱动程序的,有没有相关例程?

  • Qing Gao 说:

    打算使用C67XX系列, 有如下几个问题请教下,谢谢!

    1.  MCASP和McBSP使用有什么区别?

    ---   这哪能一句话说的清,总之做为普通的I2S是一样的,mcasp的特点是有多条数据线,这样可以实现音频里的多通道音频,而mcbsp只有收发各一条.

    2. MCASP速度可以达到多少?(我指的速率是每秒传多个16bit数据);如果EMIF时钟是10M,那以16bit为一个单位的话,速度还不到1M,我看了手册上UART的速度可以达到12Mbps,这么换算的话EMIF不是速度还低于UART?如果用EMIF接口,线比较多,用那种排线的可靠传输距离是多少?

    ---- 哪有EMIF只有10MHz的?EMIF只适合于板上连接,板间要加驱动器。

    3. 674x和C6713比性能上有多大差别?价格上对比如何?

    ---- C674x 性能上要高很多,体现在指令集上,价格差别参考网上公开报价。

    4.6000系列的是不是都没有片内flash,是否需要扩展片外flash?现在我的单板外围设备就有了MCBSP接口,FLASH接口,DDR接口,UART接口或者EMIF接口或者MCASP接口,这些接口应该都要驱动程序的,有没有相关例程?

    ---  一般来说高端处理器都没有片上集成flash的。例程参考starterware包