This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在线等:关于DM368 LCD驱动的时钟



之前在dm368平台上调通了480x272的一块屏的驱动,LCD的时钟频率是27M。

现在系统换了一块新的屏,分辨率为240x320,LCD的时钟频率为10M,

LCD的频率由DM368的DCLK提供,DCLK由CLK_ENC提供,CLK_ENC为PLL1SYSCLK6,即27M,

那么怎么产生这个10M的时钟呢?

配置了DCLKCTL和DCLKPTN0,如下:

dispc_reg_out(VENC_DCLKCTL, 0x1);
dispc_reg_out(VENC_DCLKPTN0, 0x1);

理论上应该产生27/2=13.5M时钟,可示波器亮出来后CLK波形一直在抖动,好像是占空比不稳定,频率在13.5M附件不断地上下跳动,这是为什么?

关键问题是怎么产生LCD要求的10M时钟?

在线等,谢谢大家!

  • Timer,

    如果没有外部10M时钟输入,很难让VPBE输出10M时钟。请问你的LCD屏是否接受9M时钟,如果可以,可以使用clock pattern 每3个时钟,使能一个时钟,来近似获得9M时钟。

  • Chris,谢谢你的回复,下面配置后

    dispc_reg_out(VENC_DCLKCTL, 0x2);
    dispc_reg_out(VENC_DCLKPTN0, 0x1);

    DCLK大概是9M的,但这样配置CLK的时钟占空比就没有50%,量出来的波形一直再抖不稳定,不知道是否和占空比不足有关系,

    clock pattern的方式可以获得稳定的时钟输出吗