This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

问几个关于存储器的问题



1、SDRAM中PC133指什么啊。我看了MICRON的资料说PC133是指DATA RATE,和时钟频率不是一回事,DATA RATE是个什么概念。同样是PC133,时钟频率有好就几种。我一直以为PC133是指SDRAM工作在133MHz。

3、SDRAM中是不是A10永远不会用作列地址信号。

2、为什么有的存储器有读使能信号,有的没有,是不是异步存储器一般有读时钟信号,同步的没有。异步存储器是利用读写使能信号来锁存数据和地址,同步是利用时钟。理解的对吗?

  • dawei wang1 说:
    2、为什么有的存储器有读使能信号,有的没有,是不是异步存储器一般有读时钟信号,同步的没有。异步存储器是利用读写使能信号来锁存数据和地址,同步是利用时钟。理解的对吗?

    这句话前后是一个意思吗?

    dawei wang1 说:

    1、SDRAM中PC133指什么啊。我看了MICRON的资料说PC133是指DATA RATE,和时钟频率不是一回事,DATA RATE是个什么概念。同样是PC133,时钟频率有好就几种。我一直以为PC133是指SDRAM工作在133MHz。

    ----- 同步接口,时钟就是数据率,如果是DDR,则数据率是时钟的2x .

    3、SDRAM中是不是A10永远不会用作列地址信号。

    ----- A10只是在做充电时用作了控制管脚。没说不当地址信号,如果只是用做充电而不当地址信号,何不另取一个专用的名字,比如Charge之类的。

  • 1、我知道DDR是数据率2倍时钟频率2倍,问题是MICRON的SDR SDRAM PC133就有好几种时钟频率,比如200MHz,166MHz

    3、我是说不能当《列》地址,不是说行地址。

  • 3、我是说不能当  列  地址,不是说不能当行地址,因为充电命令和列地址是同一个时钟周期发出的,所以不能当列地址,否则就冲突了。

    1、MICRON 的”SDR“ SDRAM容量64Mb的DATA RATE为 PC133可是时钟频率有好几种啊,比如200MHz,166MHz,官网上就能看到。

    2、我就是想知道为什么有的存储器有读使能信号,有的没有。

  • PC133:  https://en.wikipedia.org/wiki/PC133

    https://en.wikipedia.org/wiki/Synchronous_dynamic_random-access_memory#SDR_SDRAM

    Addressing (A10/An)[edit]

    Many commands also use an address presented on the address input pins. Some commands, which either do not use an address, or present a column address, also use A10 to select variants.

    Both read and write commands require a column address. Because each chip accesses eight bits of data at a time, there are 2048 possible column addresses thus requiring only 11 address lines (A0–A9, A11).


    应该说是读写信号分开,还是读写信号合一,比如SDRAM的读是WE为高,当然同时结合CAS信号。

    这些东西都是相应的JEDEC标准制定的.