This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467T HPI和NAND复用问题



1、如果HPI和NAND要复用,在硬件设计上是否要加选择芯片实现分时复用,还是可以直接通过HPI及NAND各自的片选择信号来实现,另外对于一些复用的数据线是否可以直接和HPI及NAND的数据线相连,如果直接相连会不会影响逻辑。
2、复用时可否用软件控制
3、另外DM368和DM6467的SPI接口速率是多少?
4、7/2我发表的“DM6467T接口”帖子,你们一直没有回复,请问是不知道还是正在研究?

  • 复用的pin,如果要用不同的功能的情况只能分时,但是软件以及硬件信号逻辑要仔细处理,否则会有很多问题.

    关于问题3请根据datasheet中时钟源以及clock限制计算.

    关于问题4看了帖子回答的比较清楚了,不知还有什么疑问?请仔细研究一下