This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: RTOS example program main_temperature_sensor.c, I2C data sequence contains significant delay

Part Number: AM3359
Other Parts Discussed in Thread: SYSBIOS, AMIC110, AMIC120

Hello Experts,

AM335x Beaglebone Black development board, PROCESSOR-SDK-RTOS-AM335X Version: 06.03.00.106, example project  main_temperature_sensor.c.    modified to suit my slave device.

slave device address 0x48 

modify to slave device  register address (0x01)

read from slave device with 2 bytes,

enable I2C1  (P9_17 and P9_18)

modify to run @ 400Khz

from Oscilliscope (read 2 bytes from slave device)

| START | 0x48 | write=0 | 0x01 | huge delay | 0x48 | read=1 | byte1 | byte2 | STOP | huge delay |

400khz.jpg

Please help. thanks in advance

 

/**
 *  \file   main_temperature_sensor.c
 *
 *  \brief  Example application main file. This application will get the
 *          temperature from the temperature sensor through I2C interface and
 *          displays on the serial console.
 *
 */

/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Error.h>

/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>

#include <stdio.h>
#include <string.h>

#include <ti/drv/i2c/soc/I2C_soc.h>
#include <ti/drv/i2c/test/eeprom_read/src/I2C_log.h>
#include <ti/drv/i2c/test/eeprom_read/src/I2C_board.h>

#include <ti/csl/hw_types.h>
#include <ti/csl/soc.h>

#define CM_PER_I2C1_CLKCTRL     (SOC_CM_PER_REGS + 0x48)

static void enableI2C1Module(void)
{
    /* Enable I2C1 clock in CM_PER */
    HWREG( CM_PER_I2C1_CLKCTRL) = 0x2;   /* MODULEMODE = ENABLE */
    while ((HWREG( CM_PER_I2C1_CLKCTRL) & 0x30000) != 0) {
        ; /* Wait for MODULEMODE to become functional */
    }

    /* Configure I2C1 pins manually (BBB: P9_17=SCL, P9_18=SDA, mode 2) */
    HWREG(0x44E10958) = 0x72;   /* conf_uart1_rxd -> I2C1_SDA, mode 2, pull-up, receiver enabled */
    HWREG(0x44E1095C) = 0x72;   /* conf_uart1_txd -> I2C1_SCL, mode 2, pull-up, receiver enabled */
}


/* Temperature sensor slave address */
#define I2C_TEMP_SENSOR_SLAVE_ADDR     (0x48U)

/* Instance of I2C controller that is connected to the temperature sensor */
#define I2C_TEMP_SENSOR_INSTANCE       (1U)

#define I2C_TRANSACTION_TIMEOUT         (2000U)

/**********************************************************************
 ************************** Global Variables **************************
 **********************************************************************/
/*
 *  ======== Board_initI2C ========
 */
static void Board_initI2C(void)
{
    Board_initCfg boardCfg;

    boardCfg = BOARD_INIT_PINMUX_CONFIG |
        BOARD_INIT_MODULE_CLOCK |
        BOARD_INIT_UART_STDIO;
    Board_init(boardCfg);
}

/*
 *  ======== test function ========
 */
void i2c_test(UArg arg0, UArg arg1)
{
    I2C_Params i2cParams;
    I2C_Handle handle = NULL;
    I2C_Transaction i2cTransaction;
    uint8_t txBuf[1] = {0x01};
    uint8_t rxBuf[2] = {0x00, 0x00};
    int16_t status;
    int i=0;

    I2C_log("\n I2C Temperature Sensor Application \n");

    I2C_init();

    I2C_Params_init(&i2cParams);
    i2cParams.bitRate = I2C_400kHz;   /* Use predefined macro */

    handle = I2C_open(I2C_TEMP_SENSOR_INSTANCE, &i2cParams);

    while(1)
    {
        I2C_log("\n\r");

        I2C_transactionInit(&i2cTransaction);
        i2cTransaction.slaveAddress = I2C_TEMP_SENSOR_SLAVE_ADDR;
        i2cTransaction.writeBuf = (uint8_t *)&txBuf[0];
        i2cTransaction.writeCount = 1;
        i2cTransaction.readBuf = (uint8_t *)&rxBuf[0];
        i2cTransaction.readCount = 2;
        i2cTransaction.timeout   = I2C_TRANSACTION_TIMEOUT;
        status = I2C_transfer(handle, &i2cTransaction);

        if(I2C_STS_SUCCESS == status)
        {
            for (i = 0; i < 2; i++)
            {
                I2C_log("\n Byte %d: 0x%02X \n", i, rxBuf[i]);
            }
        }
        else
        {
            UART_printStatus("\n Some tests have failed. \n");
        }
    }

    I2C_close(handle);

    while (1) {
    }
}

/*
 *  ======== main ========
 */
int main(void)
{
    Board_initI2C();
    enableI2C1Module();    /* enable I2C1 */

#if defined (SOC_AM335X) || defined (SOC_AM437x)
    Task_Handle task;
    Error_Block eb;

    Error_init(&eb);

    task = Task_create(i2c_test, NULL, &eb);
    if (task == NULL) {
        System_printf("Task_create() failed!\n");
        BIOS_exit(0);
    }
#endif

    /* Start BIOS */
    BIOS_start();
    return (0);
}