This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM8107编码1080P导致网络ping不通的问题



大家好:

最近在使用DM8107芯片做1080P的编码是出现了一个问题:编码1080P时偶尔会出现网络ping不通的情况,我的usecase如下

capture->dei->nsf->merge->ipcOutVpss->ipcInVideo->enc->A8,在A8上不对数据做任何处理(无后续操作),可以确定不是A8上的程序导致的,

测试后发现编码小于1280X1024的分辨率是不会出现上述问题的。

这是芯片模块工作的频率:

ARM clk: 1000MHz
DDR clk: 533MHz
L3 clk: 240MHz
IVA clk: 450MHz
ISS clk: 560MHz
DSS clk: 260MHz
DSP clk: 750MHz

请问可能是哪里导致的这个问题,谢谢。附件是ping超时的截图