你们为什么不回帖呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
稍安勿躁,windows的环境就是很多问题,那就是最好换到win7了
这个文档我都快背下来了。我一直是照着这个做的。。我现在就是想确定到底是硬件的问题还是spl的问题:
1关于硬件,这个板子是我自己画的,也许会出现一些硬件问题,但是现在能够下载spl进去,
2uboot问题,因为我的板子上没有EEprom,所以我也按照TI工程师的要求,修改了EEPROM的程序,以及DDR3,和PINMUX的程序。
电路上的设计,应该用USB0接口,并按照我们的beaglebone black的usb电路进行设计。
方便的话,你也贴贴你的usb部分电路
您好,这是我的USB电路:
下面是串口的打印信息的出错部分:
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB1 Peripheral mode controller at 47401000 using PIO, IRQ 0
Using default environment
usb_ether
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 80:30:dc:95:a9:81
HOST MAC de:ad:be:af:00:00
RNDIS ready
musb-hdrc: peripheral reset irq lost!
ERROR: The remote end did not respond in time.
at ether.c:2400/usb_eth_init()
Problem booting with BOOTP
### ERROR ### Please RESET the board ###
对了,我甚至按照BBB的板子,将上图中的R25改为0欧,将R78和R79也都改为0欧了
手头有没有BBB的板子,可以拿过来测试下到底是硬件的问题还是软件的问题。