This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: RTOS的tidl_model_import.out支持双输入么?

Part Number: TDA4VM

RTOS的tidl_model_import.out支持双输入么?

目前的配置文件

tidl_import_yolox.txt

modelType          = 2
numParamBits       = 16
numFeatureBits     = 16
quantizationStyle  = 3
quantizationLevel  = 4
memPoolSizeL3      = 1073741824   
memPoolSize        = 134217728    
inputNetFile       = "../../test/testvecs/25025test/250525_op11_forced.onnx"
outputNetFile      = "../../test/testvecs/25025test/output/25025_tidl_net_SDK9_1.bin"
outputParamsFile   = "../../test/testvecs/25025test/output/25025_tidl_io_SDK9_1.bin"
inDataNorm         = 1
inMean             = 8 8 8 8
inScale            = 0.001988 0.001988 0.001988 0.001988
inDataFormat       = 1
inWidth            = 1080
inHeight           = 1920
inNumChannels      = 4
numFrames          = 20
inData             = "../../test/testvecs/25025test/detection_list.txt"
perfSimConfig      = ../../test/testvecs/25025test/device_configs/j721e_config.cfg
debugTraceLevel    = 2

 

模型*.onnx信息

(tidl_9.1) wp@wp:~/jm/tda4vm/download/ti-processor-sdk-rtos-j721e-evm-09_01_00_06/c7x-mma-tidl/ti_dl/test/testvecs/25025test$ python3 onnx_check.py
Opset: 17
Operators: ['Add', 'Clip', 'Constant', 'Conv', 'ConvTranspose', 'LeakyRelu']
Input: current_frame [1, 4, 1080, 1920]
Input: pre_fusion [1, 4, 1080, 1920]
Output: denoise_img [1, 4, 1080, 1920]
Output: fusion_img [1, 4, 1080, 1920]

 

 

执行和还原现场信息:

使用./out/tidl_model_import.out ${TIDL_INSTALL_PATH}/ti_dl/test/testvecs/25025test/tidl_import_yolox.txt

无法正常执行,输出结果。

执行现象如下:

(tidl_9.1) wp@wp:~/jm/tda4vm/download/ti-processor-sdk-rtos-j721e-evm-09_01_00_06/c7x-mma-tidl/ti_dl/utils/tidlModelImport$ ./out/tidl_model_import.out ${TIDL_INSTALL_PATH}/ti_dl/test/testvecs/25025test/tidl_import_yolox.txt
ONNX Model (Proto) File  : ../../test/testvecs/25025test/250525_op11_forced.onnx
TIDL Network File      : ../../test/testvecs/25025test/output/25025_tidl_net_SDK9_1.bin
TIDL IO Info File      : ../../test/testvecs/25025test/output/25025_tidl_io_SDK9_1.bin
Current ONNX OpSet Version   : 11
Running tidl_optimizeNet
tidl_model_import.out: tidl_import_common.cpp:201: void* my_malloc(int): Assertion `ptr != NULL' failed.
已中止 (核心已转储)
(tidl_9.1) wp@wp:~/jm/tda4vm/download/ti-processor-sdk-rtos-j721e-evm-09_01_00_06/c7x-mma-tidl/ti_dl/utils/tidlModelImport$ 

 

 

问题:

tidl_model_import.out不支持多输入的模型么?