This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于6630K2L的高速接口的几个问题!!!

Other Parts Discussed in Thread: RFSDK

各位专家:

大家好,我有几个6630k2l的高速接口的几个问题,请大家帮助!

1、基于数据流方式的高速接口

6630K2L芯片的高速接口包括AILJESD等,均是基于数据流的高速接口。数据流的方式系统延时更小,而数据包的处理方式延时较大。TI66706630的接口变化上,取消基于包传输的SRIO接口,加强基于数据流的接口CPRIJESD等,视乎是在提升系统延时方面的功能。但是66706630DSP的高速协处理器、DMA等结构,视乎更适合进行基于大数据块和包的处理(数据块越大,系统处理效率、DMA搬移效率越高)

请问如何在66706630这样的多核DSP中实现类似数据流方式的处理, 而不降低整个系统的处理效率呢?

26630K2LCPRI的问题

6630K2L芯片中,IQN2接口可以通过可通过两个AIL接口实现与FPGA的接口,该接口可支持CPRI协议。请问6630K2L芯片在使用AILFPGA进行CPRI通信时,

是否可作为从端进行通信,其从端时钟恢复功能在哪里体现?

若进行硬件设计,6630FPGA在板内通信,两端CPRI时钟可直接共源,以简化FPGA侧时钟恢复电路设计。

请问 6630CPRI处理时钟在哪里?以便外接到FPGA

36630K2LDFE接口的问题

DFE模块是否能屏蔽其中的收/发数字信号处理功能,而仅作为一个高速通道实现DSPFPGA直接的JESD高速接口功能?具体该如何实现?

46630K2LDFE的均衡器问题

DFE中的RX模块中的均衡器,是否用于物理层信号处理的时域均衡,均衡抽头的产生6630中是否提供算法,即根据信道变化自动收敛,并不停的产生新均衡抽头系数?

请各位专家提供帮助,非常感谢!!!