公司自己开发的单板,带双网口、双CAN。内核linux-3.2.0-psp04.06.00.11
pinmux配置:
static struct pinmux_config d_can_gp_pin_mux[] = {
{"uart1_rxd.d_can1_tx", OMAP_MUX_MODE2 | AM33XX_PULL_ENBL},
{"uart1_txd.d_can1_rx", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
{NULL, 0},
};
static struct pinmux_config d_can_ia_pin_mux[] = {
{"mii1_txd3.d_can0_tx", OMAP_MUX_MODE2 | AM33XX_PULL_ENBL},
{"mii1_txd2.d_can0_rx", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
{NULL, 0},
};
系统启动后CAN1通讯正常,CAN0收发都不通。
用USBCAN连接单板调试,刚上电时,K15引脚上的波形正常,但是系统出现下面的打印信息后,信号低电平由0V变成2V。
[ 1.603250] can: controller area network core (rev 20090105 abi 8)
[ 1.609873] NET: Registered protocol family 29
[ 1.614619] can: raw protocol (rev 20090105)
[ 1.619120] can: broadcast manager protocol (rev 20090105 t)
[ 1.625137] Registering the dns_resolver key type
[ 1.630177] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.638265] ThumbEE CPU extension supported.
在早先的一款只支持单网口的单板上,双CAN口工作都没有问题。新开发的单板因为要支持双网口,进行过一次内核升级。
请问这一故障有没有可能是受双网口影响产生的?
是否需要修改驱动?