DM8127上可以用eMMC做存储吗?比如说取代FLASH或者SD卡?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不建议用emmc作为启动设备。
4.7.4.3 Booting Procedure
The high level flowchart of the eMMC/eSD and MMC/SD booting procedure is depicted in Figure 4-17.
The booting file is searched only in case of booting from a card. eMMC/eSD embedded memories only
support raw mode.
而且DM8127上的SD/MMC支持的标准也不是很新。
The device includes 3 MMC/SD/SDIO Controllers which are compliant with MMC V4.3, Secure Digital Part
1 Physical Layer Specification V2.00 and Secure Digital Input Output (SDIO) V2.00 specifications.