This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150AM1能否解码输出画面为16:9的PAL信号

Other Parts Discussed in Thread: TVP5150

如题,CCD靶面尺寸是16:9的,输出的模拟PAL视频也是在16:9显示器上看是不失真的。那么我想问一下,16:9PAL和4:3Pal区别是不是在消隐期的不同,TVP5150能否正确的查到消隐期和像素时钟?谢谢

  • Zhang Hongyu,

    PAL的标准分辨率就是720x576,比例不是完全正好是16:9。TVP5150的输出只能是输入图像的比例,不会做任何图像宽高的修改。

  • 从你显示器上看说不失真,那么是不是显示器上有黑边的?

    我觉得你的输出的模拟PAL应该就是有加了黑边的,所以给出来的就是一个图像上含黑边的标准PAL信号而已,所以显示器(TV)可以正常显示不失真的。

  • 你好,我就是想问下,是不是只要是PAL制式的图像,TVP5150都可以正常解出行同步、场同步、场消隐和像素时钟?因为我觉得16:9的PAL信号,可能黑边(也就是每行的消隐期)会比4:3的短一点。行信息也不是576,会少一点。不知道我理解的对不对?