新手请教!
在BeagleBone Black原生态Ångström Linux系统的时候已经装过驱动,并且可以在PC上正确识别出linux网卡和自动给这个网卡分配192.168.7.1地址,然后我用SD卡做了个Ubuntu14.04的镜像,但是问题来了,USB再连上电脑的时候,系统启动,再也不能给我的这个网卡自动分配IP了,就是分配的都是169开头的IP错误地址,除非我手动设置192.168.7.1才行,请问是怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
新手请教!
在BeagleBone Black原生态Ångström Linux系统的时候已经装过驱动,并且可以在PC上正确识别出linux网卡和自动给这个网卡分配192.168.7.1地址,然后我用SD卡做了个Ubuntu14.04的镜像,但是问题来了,USB再连上电脑的时候,系统启动,再也不能给我的这个网卡自动分配IP了,就是分配的都是169开头的IP错误地址,除非我手动设置192.168.7.1才行,请问是怎么回事?
请问您是指usb模拟成网卡吗?如果这样,您的pc上有dhcp服务器吗?没有dhcp,不能动态分配ip的
你好,在原生态系统Ångström Linux的时候我的PC机和现在没有什么改动,那时候是可以自动分配IP的,看手册说是BBB本身带的DHCP,可以分配192.168.7.0-3的ip,其中192.168.7.2板卡自己用了,一般会给连接的PC分配192.168.7.1,而不是PC的DHCP分配的,我的理解对吗?