AM62P: Consultation on SDK Compilation and Download Issues for [AM62P+FreeRTOS] Platform

Part Number: AM62P


Dear Sir,

I have the following questions to consult you regarding the use of your company's AM62P platform (which is newly purchased with no additional operations performed whatsoever, including hardware adjustments and software flashing). Could you please provide guidance on these matters?
  1. I followed the steps below, but there is no any output printed on the serial port. According to your online documentation, there should be continuous 'C' characters printed.LED4 and the FTDI LED are lit normally, while the other LEDs remain unlit. There are four serial ports in total, but none of them produce any printed output.It has been confirmed that SW4/SW5 are set to uart boot mode, and the power supply is a 5V 3A USB adapter.1.png

2. Regarding the method of creating the SD card image, I have only found the corresponding Linux-related guide documents and relevant tools. 

2.png

For creating a FreeRTOS image on Windows, can I directly use Win32DiskImager to create a bootable image from the .hs_fs file?(The file name is: uart_echo_callback_am62px-sk_mcu-r5fss0-0_freertos_ti-arm-clang.appimage.hs_fs)

3.Currently, we are mainly debugging the WiFi module on the FreeRTOS system. We would like to confirm whether we can directly select the freertos_uart_echo demo project for porting.

4.For the AM62P system architecture diagram: what operating systems are running on each component respectively? What precautions should be noted during normal use? Are there corresponding images for compilation and flashing?For example, regarding the use of DM R5 and MCU R5, and additional questions as follows: 

3.png

4.png

5.Regarding the usage method of JTAG: Is a corresponding adapter board absolutely necessary for the Micro B and XDS110? Are there any specific requirements for it? Could you please provide the corresponding model? We already have an XDS110 debugger on hand and are considering purchasing the matching adapter board. 

Thanks!