This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在做6678上的EMIF Nor-Flsh启动,把程序烧写进去后,加电自启动,然后就仿真器连接,发现PC指针停留在0x700XXXXX(flash的地址空间)的位置,按照论坛上别人说的方法,我查看了bootcomplete的值为1,DEVSTAT的值为1021, boot mode寄存器的值是70,代表EMIF启动。我的flash是挂在ce0上的,现在就有一个疑问:
(1)DSP加电自启的时候,是直接跳到nor flash里面去执行前1K代码,还是先将1K代码读到片上L2,执行这1K代码将flash 1K代码之后的应用程序搬移到L2去
执行,还是直接跳转到flash里面去执行。如果是第一种,那PC指针跳到了flash的地址该如何解释呢?
(2)flash的前1K空间,除了要烧写bootloader,是否还需要烧写启动参数表boot parameter table呢
就目前的状况,应该是启动没成功,不知道问题出在哪儿,希望大牛们给帮忙指导一下,非常感谢!
DSP在运行完RBL后是直接跳到0x70000000去执行的。这段代码应该是你自己的bootloader。
你的这个情况应该是在搬移了代码后没有跳转到_c_int00导致的。
搬移程序是在bootload.asm中编写的,放在应用程序员一起进行编译,然后烧写到Flash前1KB的空间,应用程序烧写到Flash 1KB后的空间。DSP上电后,程序计数器跳转到Flash的空间执行搬移程序,搬移程序将应用程序搬移到DSP的4M共享内存上,搬移完成后,程序计数器跳转到DSP上开始执行应用程序。我现在EMIF单核和多核启动都成功了,而且非常稳定。