大家好,我想问下我用的是ti-processor-sdk-linux-am335x-evm-02.00.00.00的SDK,硬件是beaglebone black,我修改了arch/arm/boot/dts/am33xx.dtsi,将spi使能
git diff arch/arm/boot/dts/am33xx.dtsi
diff --git a/arch/arm/boot/dts/am33xx.dtsi b/arch/arm/boot/dts/am33xx.dtsi
index 3a74c2d..4ea748d 100644
--- a/arch/arm/boot/dts/am33xx.dtsi
+++ b/arch/arm/boot/dts/am33xx.dtsi
@@ -483,7 +483,7 @@
&edma 18
&edma 19>;
dma-names = "tx0", "rx0", "tx1", "rx1";
- status = "disabled";
+ status = "okay";
};
spi1: spi@481a0000 {
@@ -499,7 +499,7 @@
&edma 44
&edma 45>;
dma-names = "tx0", "rx0", "tx1", "rx1";
- status = "disabled";
+ status = "okay";
};
usb: usb@47400000 {
启动后在/sys/bus/platform/drivers/omap2_mcspi下都有看到SPI的文件,但是在/dev下没有spi*.*
想问下如何修改?