各位专家好:
GPIO16~31多功能管脚配置在PIN_CONTROL_0定义,而GPIO0~15多功能管脚配置在哪定义呢
DataSheet中只找到
(LENDIAN/GPIO[0], BOOTMODE[12:0]/GPIO[13:1], PCIESSMODE[1:0]/GPIO[15:14] and
PCIESSEN/TIMI0)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你是指GPIO复用boot mode吗?datasheet中指的就是bootmode的配置,芯片在解复位的时候会锁存这些管脚的电平到DEVSTAT寄存器,ROM boot code会根据对应的模式初始化相关外设,加载程序。在客户自己的程序中,这些GPIO可以根据需要重新使用,这就是GPIO的多功能配置。
如果你是要看GPIO的管脚功能,配置输入/输出/中断,那需要参考GPIO的手册。