This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2014年达芬奇精华帖汇总(DM36x)-硬件问题



1. 10bit raw的sensor和dm365 ipipe的配合
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61379.aspx

2. 368与Micro-SD Card的连接问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61873.aspx

3. 8127 one shot mode 说明在哪里?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/70185.aspx

4. 8127 标清模拟视频显示问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/70118.aspx

5. Appro dm368更换红外sensor
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/76616.aspx

6. appro dm368量产烧写问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/72053.aspx

7. DM365
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/66479.aspx

8. dm365 在此种硬件条件下能否通过串口得到bootme信息
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/59005.aspx

9. dm365是否支持ddr2 800?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/51820.aspx

10. dm368 14bit sensor 输入问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/70056.aspx

11. DM368 采集图形异常
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/51714.aspx

12. DM368中BOOT MODE 以及AECFG设置问题?
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61877.aspx

13. DM368中VEDIO DAC电路问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61876.aspx

14. DM368的ISIF与CMOS的连接问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61635.aspx

15. DM368的若干引脚连接问题,请大家帮忙!
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61996.aspx

16. H3A AF系统框图问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/70429.aspx

17. H3a 怎么实现自动对焦,自动白平衡,自动曝光
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/66771.aspx

18. IPNC的Dark Frame Subtraction问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61351.aspx

19. TMS320DM368 的bootloader mode 配置成NANDFLASH BOOT LOADER MODE 时,硬件配置的问题...
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/62306.aspx

20. 关于TMS320DM368的ISIF接口连接问题
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/61799.aspx

21. 对于DM368 未用I/O的处理方式。
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/62776.aspx