This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678le评估板连不上



ccs5.5

win7 64位系统

评估板上电之后 系统检测不到新硬件 上下两个评估板都是这样

  • 参考如下link设置EVM,看是否能连上仿真器。

    http://processors.wiki.ti.com/index.php/TMDXEVM6678L_EVM_Hardware_Setup

  • 按说明设置的 PC还是检测不到硬件设备 

    [Start]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\SunHui\AppData\Local\.TI\693494126\
    0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'bh560v2u.out'.
    E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
    Download failed for file C:\ti\ccsv5\ccs_base\common\uscif\xds560v2.out

    An error occurred while soft opening the controller.

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver or utilities.

    The value is '-250' (0xffffff06).
    The title is 'SC_ERR_ECOM_EMUNAME'.

    The explanation is:
    An attempt to access the named emulator via USCIF ECOM has failed.

    [End]

  • 你使用的是带子卡Blackhawk 560V2仿真器的EVM么,像是硬件连接有问题,没有检测到可用的仿真器连接,需要连接到子卡的mini usb。拍个照看看你的硬件连接。