Part Number: AM62P
We are trying to boot QNX on AM62Px using SBL OSPI boot flow, and the boot consistently fails with:
ERROR: invalid fdt address 0x00000000
This error is printed from QNX very early during A53 startup, indicating that the FDT address passed in x0 is 0x0.
During the qnxappgen image generation i can clearly see that.dtb is loaded with 0x88000000 still it's failing.
i wanted to understand wherever i have to configure the fdt load address. in config.mak file is sufficient ot load FDT?
here i will attach the issue sniipet as well as the qnxappgen build log.

Thanks,
selva